Other Parts Discussed in Thread: LMC555, LM555, NA555, SE555, TLC555, SA555
Hi team,
Is there a timer similar to NE555 and can timing to 5s~20s?
Thanks a lot!
B.R.
Zhizhao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zhizhao,
The NE555 can be used for 5 - 20s timings. Similar timers to the bipolar NE555 are the NA555, SE555, SA555, and LM555. We also have the LMC555 and TLC555 CMOS timers. All of the mentioned can be used for 5 - 20s. The Feature Description section of the datasheet gives the configurations and equations to set up the timing. You can also take a look at these FAQ posts:
Best,
Katlynne Jones