Hi all
Would you mind if we ask LMK03328?
Could you refer to the following .tcs file which is produced by TICSPRO?
■20210112_PRI=NC__SEC=TCXO27MHz___148.5MHzOUT_300MHzOUT_400MHzOUT.tcs■
20210112_PRI=NC__SEC=TCXO27MHz___148.5MHzOUT_300MHzOUT_400MHzOUT.tcs
Our customer uses these register data for EEPROM page 0 write.
However, our customer told us that using these register data, it is impossible to use I2C.
So, we persuaded to use except EEPROM page 0 like as dafault setting.
In spite of page setting, they could not access using I2C.
We can't belive it, however we would like to try it.
We would like to try it using LMK03328 EVM.
However we don't have it now.
That's why, could you try it using your LMK03328 EVM?
As the point of confirmation;
1. Write all registers to EVM with this .tcs file.
2. Program EEPROM on Page 0.
3. Cycle Power off and On.
4. After that, could you confirm whether it is impossible to access registers using I2C or not?
And then, possibly check if LMK03328 output clock when it receives 27MHz clock on SecRef.
Kind regards,
Hirotaka Matsumoto