Hi Guys,
I need your help
Our customer is using a LMX2594 on a custom board and it seems to work fine.
When they use readback on MUXOUT every register can be read back just as expected except R110 where it reads 0x0668.
Bit 4 makes no sense according to the datasheet. The selected VCO is correct concerning there application.
The lock status says it would be unlocked, even if the output waveform is perfectly fine and is stable over temperature (measured with Spectrum Analyzer).
When I set R0[2] to 1 it goes high right after programming (with all other registers kept as previous). So this not a real problem, as everything seems to be working but I am just confused by this behavior.
Hope to hear from you regarding this matter.
Thank you in advance and sincerely,
Jonathan