Hi,
I'm using the LMX2594. I am using a pulses Sysref output from the RFOUTB pins.
There is a typical application schematic in the data sheet, Figure 51. Typical Application Schematic. There are 50 ohm pull-ups on the RFOUTB pins. Is there a recommended resistor power rating to use for these? 1/16W/ 1/10W? 1/8W? It's hard to calculate the need here since i don't see what the actual output voltage swing is. Recommendations?
Thank You
Trevor