This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2430: PLL with 0~2.4V output voltage at 3GHz

Part Number: LMX2430
Other Parts Discussed in Thread: LMX2572

Hi Team,

Our customer is looking for PLL device which is similar to LMX243x series. The exact device that he needs is "A PLL, or any kind of device with pulsed voltage output with the following characteristics: 0V(gnd)~2.4V swinging voltage level, 3GHz output frequency". He would like to confirm if LMX2430TM would satisfy his requirements because the datasheet indicates that voltage swings from VOH=VCC-0.4V to VOL = 0.4V.

If the LMX243x doesn't fit his requirements, can you please suggest another device?

Regards,

Danilo