Other Parts Discussed in Thread: LMX2572
Hi Team,
Our customer is looking for PLL device which is similar to LMX243x series. The exact device that he needs is "A PLL, or any kind of device with pulsed voltage output with the following characteristics: 0V(gnd)~2.4V swinging voltage level, 3GHz output frequency". He would like to confirm if LMX2430TM would satisfy his requirements because the datasheet indicates that voltage swings from VOH=VCC-0.4V to VOL = 0.4V.
If the LMX243x doesn't fit his requirements, can you please suggest another device?
Regards,
Danilo