I'm using CDCUN1208LP in PINS mode configuration. The input LVCMOS from a clock generator ABLJO-120 at 120 MHz is direct connected with input (lvcmos)
The device seems work fine, but if I turn off my board and then turn on it the CDCUN1208LP hangs and not output is provided on any output.
The failure continue for a long time, but if I keep the board off for 2 hours about the device works. Very strange.
I checked the power supply and 3.3V came before the 1.8V
I prefer to use the device in pins configuration mode, but I can try to use it by I2C configuration if needed
Have someone any suggestions?
Thanks in advance