Good afternoon
The data sheet for the LMX2594 (page 54) shows internal 50 Ohm resistors which are not in fact there, from your comments I understand these are actually high impedance.
It also shows that with a single ended clock no coupling capacitor is required. However, this contradicts the information given on page 5 (below). Which is correct?
I have a CMOS clock and am currently assuming that I do not need the coupling capacitor or any 50 Ohm pull up but simply connect the clock outputs directly to the LMX2594 OSCin pins. Am I correct?
Many thanks for your help.