在使用ADS1146时,仅配置 SYS0寄存器,配置为0x19,然后读取次寄存器,也是0x19.启动连续转换,等待转换完成,读取数据。读取到的数据一直是0x7fff。实际万用表测量输入引脚电压为1.67V,基准电压为2.49V。如果配置寄存器 MUX1为 0x02 时,读取到的数据转换成电压为 2.49V。再次将 MUX1配置为 0 时,读取到的数据依然是0x7fff.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用ADS1146时,仅配置 SYS0寄存器,配置为0x19,然后读取次寄存器,也是0x19.启动连续转换,等待转换完成,读取数据。读取到的数据一直是0x7fff。实际万用表测量输入引脚电压为1.67V,基准电压为2.49V。如果配置寄存器 MUX1为 0x02 时,读取到的数据转换成电压为 2.49V。再次将 MUX1配置为 0 时,读取到的数据依然是0x7fff.
HI Yongqiang,
It appears this question was asked twice, so I will close out this thread and answer in the other one:
-Bryan