ADS8866 datasheet only specifies the max. operating ambient temperature Ta, but not the max. Junction Temperature Tj.
What is the max. permissive junction Temperature Tj of this part?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADS8866 datasheet only specifies the max. operating ambient temperature Ta, but not the max. Junction Temperature Tj.
What is the max. permissive junction Temperature Tj of this part?
Hello Walter,
The device consumes very little power. The junction temperature will be less than 1deg C different than the operating ambient temperature of the device.
You can use the maximum ambient temperature of 85C as the maximum junction temperature.
Regards,
Keith Nicholas
Precision ADC Applications