This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J42: Sample register cfg file

Guru 11480 points
Part Number: ADS54J42


Hello,

My customer wants to use the ADS54J42 under the following conditions.

    - Real input, Bandwidth=200MHz

    - CLKIN = 491.52MHz

    - K=32, LMFS=4211, Lane rate=4915.2Mbps, SYSREF=3.84MHz

    - Decimation = Not used

Could you please provide a sample register configuration file?

Thank you.

JH