Part Number: ADS7842
Respected sir,
With respect to above diagram we are working on a project, which requires ADC IC.
we have few quires which we would help us proceed, the quires are as follows
1. As shown in the above picture Pin 28 is analog input and pin 27 is the digital input, Is it necessary to give a analog input to the IC to work normally for ADC conversion?
2. If dc voltage(3 -5V) is applied to pin 27,while pin 28 will be in floating state what will be the output in this scenario?
3. If short circuit of Pin 27 and pin 28 with capacitors shown above in the picture, if the DC input is given will the stable output would be obtained?