Other Parts Discussed in Thread: TPS60403, LM27762, TPS61220
I'm revisiting this project. I have the ADS1262 working with my loadcell on a 0-5v supply, but would like to run it off a single cell battery.
I found this document:
www.ti.com/.../sbau206a.pdf
It shows +2.5v by a TPS79225, and -2.5v by a TPS72325. Digging further, a TPS60403 gives unregulated negative voltage to the TPS72325.
First question: Is this a power-efficient setup, and sufficiently clean for the voltages to the ADS1262? Or should I go with the suggestion of a LM27762 from the first linked post below, or a TPS61220 to boost the voltage from the 2nd post below?
Second question: Here's my schematic attempting to replicate the TPS72325/TPS79225 from that reference design. Previously I had pin #7 on the ADS1262 tied to the same ground as everything else. Now I'm separating those entirely so VSSA is tied to -2.5v from the TPS72325 and VDDA is tied to +2.5v from the TPS79225. In particular, the loadcell connection is now +/-2.5v from those same sources. Does this look right? I'm still a bit confused with the REFOUT and AINCOM pins, but those seem to work in my existing 0-5v configuration (and are unchanged in this schematic)
Related posts: