The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOST-DAC8568: 5V output

Part Number: BOOST-DAC8568
Other Parts Discussed in Thread: DAC8568, DAC8568EVM, MSP430F5529

Hello Guys,

Schematic of BOOST-DAC8568 shows it uses the 'A' variant with 2.5V output. Is it possible to make it into 5V by replacing IC on the board with other variants of DAC8568?

Or is there a module similar to the BOOST-DAC8568 that uses a C or D variant?

Thanks and regards,

Art

  • Hi Art,

    Yes, you can order a sample of either the C or D variant of the DAC8568 along with the BOOST-DAC8568 and swap the devices yourself. It looks like the DAC8568EVM does use the C variant, but this is not a BoosterPack that can connect with the MSP430F5529 LaunchPad. However, you could still wire up the pins of the LaunchPad to the corresponding pins of the DAC8568EVM.

    Best,

    Katlynne Jones