Other Parts Discussed in Thread: ADS1278, ADCPRO
Is it possible to interface and run the ADS1278 evaluation board using python scripting instead of the ADC Pro software or is there a way to initiate script based commanding using the software?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it possible to interface and run the ADS1278 evaluation board using python scripting instead of the ADC Pro software or is there a way to initiate script based commanding using the software?
Hello Steven,
Welcome to the TI E2E Community!
Unfortunately, there is no way to write your own scripting language for this evaluation platform. The ADCPro software GUI and the MMB0 data capture card are a closed system.
The ADS1278 is a simple device to communicate with. There are no internal registers; all modes of operation are configured with hardware pins. You can interface to a standard SPI port for data rates less than or equal to 105,468sps (Fclk=27MHz).
Regards,
Keith Nicholas
Precision ADC Applications