This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8887: supported SPI modes

Expert 6470 points
Part Number: ADS8887


Hi team,

which SPI modes (0,1,2 or 3) are supported by ADS8887? We guess it's mode 0, but there's no exact info on this in the datasheet.

Thanks a lot.

  • Hello Bart,

    You are correct; ADS8887 SPI mode is SPI-00.  It launches the MSB on the falling edge of CONVST(3-wire) or DIN(4-wire), and launches the remaining data bits on the falling edge of SCLK.  The host typically will capture data on the rising edge of SCLK.

    Regards,
    Keith Nicholas
    Precision ADC Applications