Other Parts Discussed in Thread: ADS1262, ADS1235, ADS125H02, ADS125H01
Hi there,
I am using the ADS1255 to measure an amplified signal from a load cell.
Normally I would measure between 0-5V BUT some Loadcells output zero offset voltage to max -150mV (so -150mV to + 5V) and I need to measure this.
I am using your recommended basic connections like in your datasheet, but AIN0 is a single ended input and AIN1 is floating.
My question now: Is it possible to measure this -150mV with this connection? I guess ADS1255 max. can measure 0V because it only is supplied with 0-5V ?!
Normally I set the channel on AIN0 as AINp Input and reference AINn is on AINCOM on GND.
Is it possible to set the channel AINp on AINCOM on GND and AIN0 on AINn to measure this small negative voltage?
Thank you for your help.
Kind Regards,
Lukas