Part Number: ADS1256
Other Parts Discussed in Thread: PGA116, ADS1255, INA849,
I need to convert low voltage differential signal (bridge circuit), some in 10mV range and some in 3-4 mV range, at about 500 samples per channel. Due to low voltage, to reach near FS, I need gain of more than 128 which is not available as integrated PGA as far as I know. Also, to reduce development time, as much as possible, I am looking to incorporate more widely used ADCs with existing libraries.
And ADS1255-56 seems like a good choice because it is widely available in breakout board form as well as has good sampling speed. But the big issue with ADS1255-56 is that the gain is only 64x. So can I use external PGA such as PGA116 with MUX as frontend to ADS1255-56 and run the ADC as single channel? First the PGA with MUX will convert differential signal to single ended ones. Then the semi amplified single ended signal will be fed to ADC where it wll be further amplified to achieve it's FS and processed.
What would be the drawbacks of such design? Would I introduce more noise or even if it is not exactly feasible?