Hi,
My device uses ADS1298, and everything runs OK. The data collect is OK. I have used it for several years.
Recently, I find that when the ADS1298 is started by writing the ADS_START (0x08) command, the first data read after start is "0" for all of the 8 channels.
After that, everything runs OK forever.
That only happens at the first frame I got after writing the ADS_START (0x08) command.
And the status word in the first frame after falling edge of DRDY pin is not "1100", what I get is "0000".
In fact, the 27 bytes in the first frame are all 0 after the first falling edge of DRDY.
Is that common for ADS1298?
Thank you.