This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ2700EVM: ADC12DJ2700EVM Lacks Documentation with my specific Board, Where Can I get my Docs?

Part Number: ADC12DJ2700EVM
Other Parts Discussed in Thread: LMK04828

I have a ADC12DJ2700EVM Evaluation Board that is of a different layout than what documentation is available on line. The online documentation which is for an ADCxxDJXX00 Evaluation Module, slau701a.pdf has a different layout than my physical board. If you look at the pdf per Figure 1-1 it shows a form factor shaped like a "T". My board is "L" shaped, Red color as well but with the dimensions on the long side of 6.25 inches, width of 3.75 inches, and on the parallel side for the 6.75 inches the other side has a notch that is 0.75 inches in size which makes it into an L shape as opposed to a "T". I suspect there is one schematic for the different Eval Boards, but I would hope there are multiple layouts and user guides. For the pdf file it shows J22  (LMKCLK) on the right hand side but for my board it is in the Center of the board near J34 and J35. So my board's layout doesn't at all agree with the documentation. Note my board has the silkscreen etch of HSP001E1. 

Where do I find the documenation for my board? Note we purchased this board several years ago and I do not have the delivered documentation.