I Have connected AVDD to 10Volts. And digital pins are connected to ESP32 which works at 3.3V digital levels. In the program, whatever value I set to DAC, the current suddenly shoots to 100mA and IC gets hot. If there is no command given to DAC7750 for setting current, the current remains at 0mA.