Hello TI team,
During the design verification we have countered issue with the sampling rate with one of he ADS1298R IC.
We are working on 500 SPS, and one of the systems have failed on the sampling rate tests, it gives ~488[Hz] consistently, and we have checked the RDY signal and it really seems that the problem is with the ADS.
Any chance we can know what is the problem with this IC? according to the ADS datasheet, the internal oscillator (clock) accuracy is +-0.5%., and we see that it is not the case here.
Our software is verified with another ADS IC and it seems to work well
.
Attaching screenshot for the RDY signal that shows that the sampling rate is ~488 [HZ].
10.24[msec]/5[pulses]=2.048[msec].
SR [Hz]=1000[ms]/2.048[msec]=488.28125[Hz]
Best Regards,
Muhammad