Part Number: DAC7716
Other Parts Discussed in Thread: TMUX6136
Hello,
I am considering the circuit using DAC7716.
I consider referenece voltage circuit to REF-A input pin on DAC7716.
Reference voltage circuit will use REF5050, REF5025, and TMUX6136.
The analog switch IC TMUX6136 is used for switching of reference voltage of 2.5V or 5.0V to REF-A input pin on DAC7716 at the initialization timing .
The internal gain setting of DAC7716 will use only x4.
And output voltage ranges of DAC7716 will +/-10V, +/-5V, and 0V to +10V. (AVDD = +15V and AVSS = -15V)
Control signal for TMUX6136 (SELx) is provided from GPIO output on DAC7716.
I'm thinking of using an analog switch IC TMUX6136 to switch the reference voltage, but I need advice on whether or not this will cause problems with the operation of the DAC7716.
Regards,
MESH