Ads8332 abnormal heat, power configuration after the completion of the pin pull high CLK will have a chance of abnormal heat, seek explanation
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ads8332 abnormal heat, power configuration after the completion of the pin pull high CLK will have a chance of abnormal heat, seek explanation
Hi Chengxin,
Are you certain you are hitting the current limit of the LDO? If not, have you been able to measure the current consumption during this fault event?
Can you please give some more details on the problem you are seeing and the conditions that lead to it? It sounds like this only happens some of the time. It is possible depending on the startup characteristics that you are latching the internal absorption device, but this will generally damage the device if this occurs. After this fault occurs, does the ADC still operate normally after restarting?
Best,
Zak