Other Parts Discussed in Thread: ADS7128
Hello all,
I recently got back from the fab house our custom PCB that features a couple of TLA2528. Like any other part, before you make a decision whether to use it or not, you take a peek at the datasheet. Well turns out the datasheet for this part was a lazy copy-paste from the ADS7128 or similar product and half the features are not available, at least that's what I'm starting to realize.
This is causing a major delay in the deployment of our company's hardware, not to mention we might have lost a few thousands in the process.
Would someone be able to clarify/fix the datasheet? How does OSR works?? At this point, I can't trust what I'm reading anymore as I'm having issues trying to read values from it.
I'm getting 0 ADC count from 0-5V inputs and 4095 counts from some thermistor ready inputs (10kohm voltage divider to a 3.3V rail) which is what I expected. As soon as I add a sensor to any of the inputs, the ADC counts for the input start to jump all over the place in the full 0 - 4095 range. It doesn't make sense, if the timing of the i2c is wrong, I would expect to get garbage on the inputs with nothing connected to it but I'm getting the expected counts.
I'm following the manual mode procedure listed below

Anyone can help with this, I will greatly appreciate some insight?
Kamil