This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5482: Reference voltage at input voltage

Part Number: ADS5482

Hi Ti team 

we are using ADS5482 ADC in our design. our signal BW is 500khz to 20Mhz . ADC clock freq is 105Mhz(LVDS), we are running ADC on 105MSPS.  We are using internal reference voltage.

But when I probed on the input pin from the multimeter its input reference pin voltage is not constant and fluctuating between 0v to 3.1V . For stable output from ADC ,its reference voltage at input voltage should be stable 3.1V. Why this is happening ?

PFB image of ADC front end input pin circuitry 

PFB ADC Schematics image

PFB decoupling cap image

Please suggest some review points to fix this problem.