This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC09QJ1300-Q1: About ADC09QJ1300-Q1 some application question.

Part Number: ADC09QJ1300-Q1


Hi team,

I have some questions about ADC09QJ1300-Q1 as below. thanks 

1. Is the sampling rate 1.3GSPS / @9bit per channel?

2. Can I use ADC09QJ1300-Q1 If FPGA Transceiver speed is 12.7Gbps ?

3. PADC09QJ1300AAV will announce the normal version? I think  preview now

4.This device can support interleave?

  • Hi Jimmy,

    Please see my answers below.

    1. Is the sampling rate 1.3GSPS / @9bit per channel? Yes, the sample rate is 1.3Gsps @ 9 bit per channel. 

    2. Can I use ADC09QJ1300-Q1 If FPGA Transceiver speed is 12.7Gbps ? Yes you can use JMODE9 or JMODE10 where your serdes rate will be lower than 12.7Gbps with sampling at 1.3Gsps.

    3. PADC09QJ1300AAV will announce the normal version? I think  preview now. You want the automotive version or the industrial version? They all should be out by end of September. 

    4.This device can support interleave? This ADC is not interleave. 

    Regards,

    Neeraj

  • Hi Neeraj,

    Thanks, I got great support.