1. Configure the negative voltage pins of the ADS126 acquisition terminal as AINCOM:GND, and configure the positive voltage pins as AIN1 and AIN0 respectively. The voltage can be stably measured as -2.499V and 2.499V.
2. Configure the negative voltage pin of ADS126 acquisition terminal as AINCOM:GND, and the positive voltage pin as AIN2. The measured data is shown in the following figure, with large deviation (the actual input waveform is relatively stable square wave).
3. The specific configuration of ADS1262 is as follows:
Chop on, PGA on, PGA gain 1V/V, 1200 SPS, Sinc1 mode, full-scale Calibration Registers:0C75ba
4. Summary of problems:
(1) The voltage drift collected by the pin of the digital filter is very large, how to configure the register to solve it?
(2) How to accurately determine the gain coefficient and migration coefficient (for calibration)