Other Parts Discussed in Thread: ADS1202, AMC1304M25
Hi team,
Digital filtering is currently being attempted using DFSDM in STM32F7, with filter inputs supporting SPI, Manchester encoding, PDM, and parallel inputs.
Customer has the following questions about AMC1304:
1. What should the digital filter interface after AMC1304 be, is it the same SPI used as the ADS1202? If so, I need to read the data on the rising or falling edge.
2. Is the digital filter followed by a sin3 OSR 256? Can the processed values be read directly?
3. The datasheet says that the voltage value is calculated based on the ratio of 0 and 1 of the data stream, then does the range of this data stream refer to data over 128 cycles? Does it mean that I need to acquire values over 128 cycles and compare the ratio of 0 and 1 values?
Best Regards,
Amy Luo