Other Parts Discussed in Thread: DAC38J84
Hi,
I am using the DAC38J84 on the EVM with an Arria10 dev board and for now, the JESD part works fine. However I am facing a problem using the NCO on this DAC. For my project, I plan to use the NCO to shift the input frequencies to higher ones and I need to really control the phase of the NCO output, that is I need to have a constant time between the NCO reset assertion and the NCO output phase reset with the device clock and interpolation used.
To do that, I use the SYSREF sync source on the Mixer AB, Mixer CD and NCO Acc. Here are the steps to achieve the test that I am doing :
- Program the FPGA with an image containing a JESD204b TX.
- Establish the JESD link between the EVM and FPGA.
- Once the link has been established, disable the SYSREF syncing to the clock dividers and the and to the JESD link0
- Change the pulser to be only 1 pulse
- Use the constant input to the dac option
- Configure the NCO
- create a SYSREF pulse by using the Sysref trigger button on the EVM.
- Use the falling edge of the SYSREF pulse as trigger and capture the DAC A output.
- Monitor the time between the falling edge trig point and the point of phase disruption of the output sine.
Doing this, the time seems to vary quite a lot (up to 10ns). Is this something expected from the EVM? Is this due to the AC coupling of the SYSREF on the eval board? Is there a way to have a constant time between sysref and nco phase output reset?
Thanks!