Other Parts Discussed in Thread: LMK04806
Hello,
My customer has an issue of the ADS54J42 SNR performance degradation with thier custom board under the following conditions.
- RF input = 368.64MHz, Bandwidth = 200MHz
- CLKIN = 491.52MHz
- K = 32, LMFS = 4211, Lane rate = 4915.2Mbps
- Decimation = Not used
The left is the ADC input signal and the right is the ADC output of matlab captured from FPGA.


Please advise on the cause of the SNR performance degradation and how to solve it.
Thank you.
JH