Dear,
I have trouble in understanding how the TSW14J10 knows what FPGA it is connected to. As can be seen in the attached screenshot it identifies for me as connected to a Xilinx ZC706. However I want to use it with a Xilinx VC707. And at the moment I can also only see the ADC selection of the ZC706. How do I change this? Does this also mean the wrong bit/svf file is uploaded to the FPGA?
Besides that I was also wondering where SW5 dip switches are for? From another forum post I saw all the dip switches were to one way but for me that doesn't seem the case. Should I change this?