Hi,
I have configured for ADS124S08 for Four-Wire PT100 RTD Measurement. RREF is 1K,1%.
I got below formula for RRTD from "Four-wire PT100 RTD measurement circuit with low-side reference"
RRTD = RREF • [Output Code / (Gain • 2^23)]
Couple of questions -
1) Is RRTD is independent of IDAC current? Output Code remains same for 1mA/2mA IDAC current?
2) I see that RREF in the RRTD calculation formula. Is tolerance of RREF (1%, 0.1%) really matters for calculated value of RRTD ? As tolerance will vary from part to part resistors.