I want to acquire sampled waveforms with ADC12D800RFRB and post-process the data in Matlab R2021a (64-bit). I read some posts from over 8-years ago indicating that interfacing to the DLL requires 32-bit Matlab. Joffray Guillory even shared his Matlab code. I don't think it's worth attempting to install a 32-bit version of Matlab on my 64-bit Windows 10 computer.
QUESTIONS:
1. Is the WaveVision 5 software compatible with Widows 10?
2. Has anyone successfully interfaced to the WaveVision DLL from modern 64-bit Matlab?
3. Is it possible to export the sampled data from WaveVision 5 into a csv file?