This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7884: Could you help me confirm the ESD information of ADS7884?

Part Number: ADS7884

Could you help me confirm the ESD information of ADS7884?

  • Hello,

    The ADS7884 device does not include specific ESD information in the datasheet.  Similar devices in the family were tested with passing results to the levels below.  Be sure you include external protection to protect the device from transients greater than these levels.

    HBM:  2.5kV

    CDM:  750V

    MM:  150V