This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5675

Other Parts Discussed in Thread: DAC5675-EP

The data sheet of current-sinking D/A converter DAC5675-EP states that  "the outputs are terminated to AVDD and
have a voltage compliance range from AVDD -1 to AVDD +0.3V".
In an Analog Applications Journal, (slyt342) of 3Q 2009, it is detailed in Figure 2 that the Compliance Voltage is AVDD +-0.3V and the
"compliance voltage shown for each group of devices is the voltage range at the DAC outputs within which a device will perform
as specified. Lower voltages tend to shut down the outputs, and higher voltages have the potential to cause breakdown. Both of
these should be avoided to provide best performance and long-term reliability".
Please resolve this discrepancy.