Hi @ all,
I'm currently a bit confused about the JESD line rate, specifically the way of calculation, could you please clarify.
My understanding, so far:
Linerate = Fclk x R
by Using JMODE 0, clk 800MHz
Linerate = 800MHz x 4 = 3,2Gbps
In JMODE0 single channel operation is applied, thus sample rate is 1600Gbps, nethertheless for calculation of line rate 800Mhz is used, is this correct?
by using JMODE 10, DDC=4, clk 800MHz
800Mbps/4 = 200Mbps (after DDC)
for line rate calculation:
linerate = 200Mbps x 5 = 1Gbps?
Or
linerate= 800Mbps x 5= 4Gbps?
The same for SYSREF calculation:
My understanding was that only Fclk needs to be considered not the Frequency after DDC, ?