Other Parts Discussed in Thread: ADS124S08, ADS1261
Hi,
We're currently doing an SI simulation which includes the ADS125H02, and we're using the ads125h0x.ibs file for this. For the dout pin, this only contains a 5V model. However, we're using the part with a 3.3V DVDD supply, and it communicates with a part that is also supplied by 3.3V. So, our simulation currently shows an output level of 5V, which is too high. In practice this will not happen, since we use a different supply voltage. Is there any way to get an updated IBIS model to perform this simulation?
Kind regards, Tobias