This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLA2024: How can it control the ADC results when all the inputs are enabled, but open/floating?

Part Number: TLA2024

Hello,

My question is related to the one posted previously by cafain-san, but my customer would like to have 0V output results when all the inputs are enabled, but open/floating.  They'd like to make the condition to have 0V outputs to think about the case where the input is disconnected unexpectedly like the connector to the ADC so that they can detect such unusual case.  Would you please tell me how they should do for the inputs?  Should they add pull down resistors?  The datasheet says the FSR needs to be +/-0.256V(min), so I'm not sure how they should do.  Note that it doesn't have to be 0V, but a certain voltage will work well if it is stable when the inputs are open, but 0V should be the most stable condition.

Best Regards,

Yoshikazu Kawasaki