This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J69: Drop-in replacement with the ADS54J42

Guru 11480 points
Part Number: ADS54J69
Other Parts Discussed in Thread: ADS54J42, , ADS54J60

Hello,

My customer is using the ADS54J42 on the custom board.

They want to test with higher resolution ADCs without PCB modifications.

Can the customer use the drop-in replacement of the ADS54J69 instead of the AD54J42?

The ADS54J42 sample rate is 500MHz or less.

Thank you.

JH