Other Parts Discussed in Thread: ADC12J4000
Hi,
I am planning to use the ADC12DJ5200RF with a 3.1696 GHz sampling clock.
I found that I can use the formulas give in the ADC12J4000 Datasheet to calculate jitter requirements depending on frequency and desired ENOB.
I am wondering if there is an upper limit to which offset-frequency one should integrate the phase noise of the sampling clock in order to measure the jitter.
In my particular example, I have a clock signal with fairly strong spurious emissions at higher frequency offsets (measurement results are shown below). I will lower those with additional filtering but I am still wondering to which extend this is necessary and how these spurious would affect the ENOB. (Does the clock input of the ADC12DJ5200RF f.e. have a higher cut-off frequency from which spurious emissions no longer need to be considered?)
Thanks and kind regards!
Measurement results:
Some highlights:
Frequency offset | Power | Jitter |
792.43 MHz | -52.69dBc | 164.69fs |
1.58 GHz | -50.06dBc | 223.02fs |
3.17 GHz | -57.29dBc | 97.01fs |
7.92 GHz | -51.57dBc | 187.43fs |