we are using AMC7836 in our Design, Where we have connected power rails in the below fashion,
AVCC_AB(Pin Number:20) and AVCC_CD(Pin Number:57) --> 12V
AVDD(Pin Number:50) and DVDD(Pin Number:63) --> 5V
IOVDD (Pin Number:01) --> 3V3
From Datasheet We understand its not required to follow the above sequence,
Above snip is from data sheet page number 78.
We understand that, its not required to follow the above sequence,
Our Board power sequence will be in the below order of
12V-->3V3-->5V
Can we follow the above order ?
Also can we know, is there any maximum time of deviation for Power Sequence.
Whether can we give
Case1: 12V @0s-->3V3@10Seconds-->5V @120 Seconds
Case2: I shall be giving 12V and 3v3 but not 5V for few minutes, such as 10Minutes