Part Number: ADS1293
Other Parts Discussed in Thread: MSP430FR5738,
Hi everyone.
I need your help for this issue. I am designing a project using ADS1293 and the MSP430FR5738. I am using SPI interface to comunnicate both ICs. At first time, it was working good, giving me the data from the 3 ECG channels, but then, the ADS stopped working. I don´t believe the problem was the comunnication because there is a routine where the MSP reads the registers that were written and all ot them are good. I replaced the oscillator crystal but the problem persists. Also I monitored the voltage at DRDYB and the voltage is always 3.3 - 3.5 V. This voltage is because the pull up internal resistor is enable.
What would be the cause of this problem? is it posible that the DRDYB pin is damaged?
I will be gratefull for an answer.
Best regards.