Hi,
I bought the ads1261evm board and found something weird while testing it.
It appears that some ad-converted samples are periodically measured pretty below the expected value,
as Power Supply Power Measurement (AVDD-AVSS)/4, DVDD/4, even when measuring without connecting any pins to the input mux.
What makes this happen?
Or is this a characteristic of sigma-delta adcs?
The condition of testing and results are as follows.
1) Test Condition
- Output data rate : 14,400SPS
- Digital filter : sinc5 filter (default, when >7200SPS)
- Conversion start delay : 189us
- Reference : internal reference enabled, REFP: AVDD, REFN: AVSS
- PGA/Gain : PGA mode / 1V/V
- Input MUX : 1) (AVDD-AVSS)/4, 2) DVDD/4, 3) No connection
2) Test Result
- (AVDD-AVSS)/4
- DVDD / 4
- No connection
Thank you for your answer in advance.
Best Regards,
Youngho.