Hi,
We have a problem and trying to find the reason behind it...
In our design we are using hardware pace detection and only one channel to detect the pace maker signals . Thus, TESTN_PACE_OUT1 is used but TESTN_PACE_OUT2 is not. As still instructed in the latest datasheet (SBAS459K –JANUARY 2010–REVISED AUGUST 2015) on ADS1298R page, these pins, if unused, must be connected to AVDD. In our design we did connect TESTN_PACE_OUT2 to AVDD.
While trying to get our design work, we noticed that our AVDD is -0.690v rather than +2.5v. We disconnected the regulator that generates +2.5v from the system, it indeed generates the expected voltage, so there is nothing wrong with it and problem is somewhere beyond generation. In our previous designs, we used to use 2 channels for pace detection and had no problem. The only difference is that TESTN_PACE_OUT2 pin is now connected to AVDD.
While looking for an explanation for this voltage level problem, I noticed that in one of the threads it is stated that TESTN_PACE_OUT2 pin should left floating when unused. I am now wondering if this could be reason behind our problem. We followed the instructions in datasheet and we worry that if there was a mistake, it is still not corrected.
I will be glad if you please make a comment.
Best regards,
Denin