hi,
I would like to use the Long Transport Test Pattern, however I cannot follow the calculation of the data.
so I'm using JMODE16 , K=20
I get:
Frame0 Frame1
DA0 (I0) = 0x0003 0x0002
DA1 (I1) = 0x0002 0x0005
DA2 (Q0) = 0x0004 0x0002
DA3 (Q2) = 0x0004 0x0004
I'm not sure if this is correct or not.
so I would expect in DA0 & Frame0:
0x0001
as AI has CID=0 => CID+1= 0x0001
or how to calculate the corresponding data??
many thanks in advance