This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS4225: Negative voltage -0.6V on INx pins

Part Number: ADS4225

Hi Expert, 

Customer found the negative voltage -0.6V on INx pins during startup transient.

It is over absolute maximum voltage(-0.3V). Is there the diode between INx pins and GND?

The input pin has a 100ohm series resister to limit input current.

Will this negative voltage have any risk?

 

Thanks

Muk