Other Parts Discussed in Thread: CC3220SF, ADS8588S
Hi Team,
I am trying to develop an ADC circuit using ADS8586S, attached will be the schematic I developed. Could you please review it? While developing the schematic I came across certain doubts, they are
1. Can I use same supply for both AVDD and DVDD (say +5V), Since both of their ranges specified in data sheet are within -0.3V to +7V?
2. Is there is any problem for using common ground for all connections? I heard something about separate grounding should be required for analog and digital pins ?
3. How can calculate and develop the required power supply (AVDD and DVDD) for my application? is there is any documents there to help me with the design?
4. Planning to connect this circuit with CC3220SF Wi-Fi via SPI. That's possible right?
I am a beginner in this field so please excuse me for the mistakes in the schematics. I referred ADS8588S schematic as my reference to this design.
I am thinking of using 250:1, 65A(rms) CT for my current measurements. Internal reference with +/-5V analog input is my aim for the design.
ARC Detection.pdfDatasheet - CT - WCM604-1.pdf
Regards,
Vineeth