Hello,
I have a custom board that is using the ADC12DJ5200RF. We are seeing some errors on the JESD link that we have been trying to resolve. It is a 2 board system with an FPGA on one board and the ADC on another. If we replace the custom ADC board with the TI Eval board we do not see errors so it seems clear there is something degraded on the custom board.
In the course of troubleshooting I was scouring these forums and found someone reference registers that are not listed in the datasheet.
Specifically they noted that they set the following:
0x4F = 0x1F
0x4D = 0x41
When I set these registers with the above settings all my JESD errors went away. This also resulted in a notable improvement in the eye diagram.
Can you explain what these registers are doing? Is there any issue with setting them different than the default value? Could I optimize my link even more with different values?
Thanks.
Mark