Other Parts Discussed in Thread: ADS1282
Using the ADS1282 Delta Sigma ADC. It is set up using a unipolar supply which the data sheet says is valid. The supply is 5.0 volts (AVDD), AVSS is 0 volts. The VREFP is 5 volts, the VREFN is 0 volts.
According to the data sheet, the input range is AVSS + 0.7 to AVDD -1.25 which is 0.7 volts to 3.75 V in unipolar mode (3.05 v range same as bipolar).
The data sheet has little information on unipolar operation. Is the output code 80000000 for 0.7v and 7FFFFFFF for 3.75 volts?